earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1
6/19/2018

Connect Agent Settings - Advanced Tab

Use the Advanced tab to configure the advanced settings of Connect Agent.

 
action_zoom_plus_stroke Advanced tab
Figure: Advanced tab

Table: Advanced Tab

Component

Description

Maximum bandwidth

Select the bandwidth at which the crash information is to be transfered. If '0' is selected, the crash information is transfered at maximum bandwidth.

  • Connect Agent Overview
  • Connect Agent Settings - Basic Tab