earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Connect Agent Settings - Advanced Tab

Use the Advanced tab to configure the advanced settings of Connect Agent.

 
action_zoom_plus_stroke Advanced tab
Figura: Advanced tab

Tabla: Advanced Tab

Component

Description

Maximum bandwidth

Select the bandwidth at which the crash information is to be transfered. If '0' is selected, the crash information is transfered at maximum bandwidth.

  • Connect Agent Overview
  • Connect Agent Settings - Basic Tab