EcoStruxure Building Operation software has a number of features that helps you increase the security in your system.
You can configure the devices that are allowed to communicate with the field server to prevent connection attempts from unauthorized devices. The IP addresses of the devices that are allowed to communicate with the field server are added to the whitelist.
Mer information finns i Firewall .
You can increase the password security by configuring a password policy that defines how passwords must be created by the users.
Mer information finns i Password Policy .
For security reasons, the default setting is for WebStation to not be embedded in another web site and for other contents to not be embedded in WebStation. However, you can change this security setting in WorkStation.
Mer information finns i Security Configuration in WebStation .
The automatic logoff function makes it possible for the system to automatically log off a user after a specified time of inactivity.
Mer information finns i Automatic Logoff .
A security banner is displayed when a user enters a secure system. The security banner notifies the user of the legal rights connected to the use of the information in the secure system.
Mer information finns i Security Banner .
The EcoStruxure Building Operation software supports certificates. Certificates are electronic credentials that are used to certify the identities of computers, and other entities on a network.
Mer information finns i Certificates .
You can increase the security between the Device Administrator and field servers using certificates and SSL security configuration.
Mer information finns i Certificates and SSL Security in Device Administrator .
To increase the security of your data, you can disable incoming HTTP communication and allow only high security communication.
Mer information finns i Encrypted Communication .
You can log all web server HTTP access to the Enterprise Server and the Enterprise Central.
Mer information finns i Web Server Access Logging .
You can log all successful and unsuccessful attempt to log on to your field server.
Mer information finns i Field Server Remote System Logging .
To prevent data transfer over the cloud server, you can disable the transfer of system information and crash information of the Enterprise Central and the Enterprise Server and its field server.
Mer information finns i Connect Agent Overview .
You can increase the security in your system by configuring the document policy. The document policy controls which file types a user can open, save, and import.
Mer information finns i Document Policy .
You can disable port 22 and the USB ports on the automation server.
Mer information finns i Disable Automation Server Ports .
Change Control is a way to require that a user add a comment and signature for changes made in the system.
Mer information finns i Change Control .