Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Seguridad
Versión del producto: 3.2, 3.3, 2022
14/12/2022

Adding a Certificate

You add a certificate to your system to increase security.

Mostrar más
action_close

The EcoStruxure Building Operation software supports certificates. Certificates are electronic credentials that are used to certify the identities of computers, and other entities on a network.

The EcoStruxure Building Operation software supports both self-signed certificates and certificates issued by a certificate authority. Certificates are included in a backup and restored on the restored EcoStruxure BMS server.

You can add an existing certificate or generate a certificate. You then activate the certificate.

The access to the certificate management in the EcoStruxure Building Operation software can be set so that certificates can only be handled by authorized users.

Default Certificates

The EcoStruxure Building Operation software uses a default certificate that only supports encryption. The default certificate is installed by default on all EcoStruxure BMS servers. When a user logs on to an EcoStruxure BMS server, the user is notified in the Security certificate risk dialog box that the certificate cannot be validated.

The user must click trust to continue to log on to the system. This dialog box cannot be turned off. The warning is displayed each time the user log on.

Self-Signed Certificate

You can activate a self-signed certificate in EcoStruxure BMS servers. The self-signed certificate can be generated in the EcoStruxure Building Operation software or in another tool.

When the EcoStruxure Building Operation software is used to generate self-signed certificates, certificates can be generated for one or many servers at the same time.

When the user logs on to the EcoStruxure BMS server with an activated self-signed certificate the user is notified if the certificate is not valid. In this case the user can choose to always trust the certificate. If trusted, the self-signed certificate's public key is stored in the certificate list in Windows. The next time the user logs on to the EcoStruxure BMS server, Windows recognizes the certificate and the user can log on without trusting the certificate again.

CA Certificates

The EcoStruxure Building Operation software supports CA certificates, certificates issued by a certificate authority. The supported file format is PEM. Each certificate can include up to three separate files.

Status of Certificate

The user can check the status of the certificate by clicking the lock in WorkStation or WebStation.

Certificates and Licensing

Certificates generated using Workstation cannot be used for licensing in SmartX servers since these certificates do not provide a root certificate or other trust chain for validation. If you use WorkStation certificates, we recommend that you generate new ones for your SmartX servers from Device Administrator when you use licensing in SmartX servers.

Para obtener más información, consulte Certificates in Device Administrator .

To add a certificate
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Security Settings .

  4. In the Security Manager Control Panel, click Certificates .

  5. In the Certificates tab, expand Certificate settings .

  6. Select the EcoStruxure BMS server where you want to add the certificate.

  7. Click Manage Certificate .

  8. In the Manage Certificates dialog box, click the Add certificate button

     
    action_zoom_plus_stroke
    .

  9. Click Add existing certificate .

  10. In the Add Certificate dialog box, in the Name box, enter a name for the certificate.

  11. In the Description box, enter a description.

  12. In the Host certificate box, enter the host certificate.

  13. In the Intermediate Certificate box, enter the intermediate certificate.

  14. In the Private key box, enter the private key.

  15. In the Password box, enter the password.

  16. Click OK .

Now that you have added a certificate, you need to activate the certificate for it to be in effect.

Para obtener más información, consulte Activating a Certificate .

  • Certificates
  • Control Panel Tab
  • Certificates Tab
  • Add Certificate Dialog Box
  • Manage Certificates Dialog Box
  • Removing a Certificate
  • Enterprise Server System Upgrade Workflow
  • SmartX Server System Upgrade Workflow