Funkcje: Bezpieczeństwo
Wersja produktu: 3.2, 3.3, 2022
2022-12-14

Activating a Certificate

You activate a certificate so it is in effect.

Pokaż więcej
action_close

The EcoStruxure Building Operation software supports certificates. Certificates are electronic credentials that are used to certify the identities of computers, and other entities on a network.

The EcoStruxure Building Operation software supports both self-signed certificates and certificates issued by a certificate authority. Certificates are included in a backup and restored on the restored EcoStruxure BMS server.

You can add an existing certificate or generate a certificate. You then activate the certificate.

The access to the certificate management in the EcoStruxure Building Operation software can be set so that certificates can only be handled by authorized users.

Default Certificates

The EcoStruxure Building Operation software uses a default certificate that only supports encryption. The default certificate is installed by default on all EcoStruxure BMS servers. When a user logs on to an EcoStruxure BMS server, the user is notified in the Security certificate risk dialog box that the certificate cannot be validated.

The user must click trust to continue to log on to the system. This dialog box cannot be turned off. The warning is displayed each time the user log on.

Self-Signed Certificate

You can activate a self-signed certificate in EcoStruxure BMS servers. The self-signed certificate can be generated in the EcoStruxure Building Operation software or in another tool.

When the EcoStruxure Building Operation software is used to generate self-signed certificates, certificates can be generated for one or many servers at the same time.

When the user logs on to the EcoStruxure BMS server with an activated self-signed certificate the user is notified if the certificate is not valid. In this case the user can choose to always trust the certificate. If trusted, the self-signed certificate's public key is stored in the certificate list in Windows. The next time the user logs on to the EcoStruxure BMS server, Windows recognizes the certificate and the user can log on without trusting the certificate again.

CA Certificates

The EcoStruxure Building Operation software supports CA certificates, certificates issued by a certificate authority. The supported file format is PEM. Each certificate can include up to three separate files.

Więcej informacji zawiera Server Certificate Workflow .

Status of Certificate

The user can check the status of the certificate by clicking the lock in WorkStation or WebStation.

Certificates and Licensing

Certificates generated using Workstation cannot be used for licensing in automation servers since these certificates do not provide a root certificate or other trust chain for validation. If you use WorkStation certificates, we recommend that you generate new ones for your automation servers from Device Administrator when you use licensing in automation servers.

Więcej informacji zawiera Certificates in Device Administrator .

Server Certificate Workflow

Use this workflow to purchase, convert and install server certificates.

Więcej informacji zawiera Server Certificate Workflow .

To activate a certificate
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Security Settings .

  4. Click Certificates .

  5. In the Certificates tab, expand Certificate settings .

  6. Click on the EcoStruxure BMS server in the server list.

  7. In the Certificate list, select the certificate you want to activate.

  8. Click the Save button

     
    action_zoom_plus_stroke
    .

The certificate is activated immediately after you save the setting.

  • Certificates
  • Adding a Certificate
  • Generating a Certificate
  • Certificates Tab
  • Enterprise Server System Upgrade Workflow
  • Automation Server System Upgrade Workflow