You can log all successful and unsuccessful attempt to log on to your field server.
The log on attempts are sent from the field server to a server that handles system logs. Two different protocols can be used to send the log on attempts:
TCP
UDP
The field server remote system logging uses a Lead shadow relationship.
That means that the setting you do on an Enterprise Server is transferred to all field servers connected to the Enterprise Server. If you log on to the field server that acts as a shadow to a lead Enterprise Server, you cannot change the field server remote system logging on the field server. Pour plus d'informations, voir Lead and Shadow Relationship .
A stand-alone field server can be configured to store logs on a central location.