earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, AS-P, Project Configuration Tool
功能: 安全
产品版本: 2023
2022/12/17

Automation Server Remote System Logging

You can log all successful and unsuccessful attempt to log on to your automation server.

The log on attempts are sent from the automation server to a server that handles system logs. Two different protocols can be used to send the log on attempts:

  • TCP

  • UDP

Theautomation server remote system logging uses a Lead shadow relationship.

That means that the setting you do on an Enterprise Server is transferred to all automationservers connected to the Enterprise Server. If you log on to the automation server that acts as a shadow to a lead Enterprise Server, you cannot change the automation server remote system logging on the automation server. 有关更多信息,请参阅 Lead and Shadow Relationship .

A stand-alone automation server can be configured to store logs on a central location.

  • Security Overview
  • Enabling Web Server Access Logging
  • Lead and Shadow Relationship