earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 安全
产品版本: 2024, 7.0
2024/12/2

Password Policy View

Use the Password Policy view to configure the password policy.

 
action_zoom_plus_stroke Password Policy view
图: Password Policy view

表格: Password Policy View

Component

Description

Minimum number of hours between password changes

Enter the minimum number of hours required between password changes. To disable this feature, enter 0. In this case, users can change their passwords immediately.

Days until password expires

Select to limit the days a password is in effect. You then enter the number of days before compulsory password change. The value of 0 specifies that the password does not expire.

Number of consecutive unique passwords before reuse

Enter the number of passwords that have to be different before you can use the same password again. To disable this feature, enter 0.

Number of characters different from last password

Enter the number of characters that must be different from the characters in the last password. To disable this feature, enter 0.

Do not allow more than three repeating identical characters

Select to allow a maximu of 3 repeating characters. To disable this feature, enter 0. 有关更多信息,请参阅 Password Policy .

Minimum number of characters

Enter the minimum number of characters allowed in a password. To disable this feature, enter 0.

Minimum of lowercase (small) characters

Enter the minimum number of lowercase characters allowed in a password. To disable this feature, enter 0.

Minimum number of uppercase (capitalized) characters

Enter the minimum numbers of uppercase characters allowed in a password. To disable this feature, enter 0.

Minimum number of numeric characters

Enter the minimum of numeric characters allowed in a password. To disable this feature, enter 0.

Numeric character must be inside password

Select to require that numeric characters cannot be the first or last character.

Minimum number of special characters

Enter the minimum number of special characters allowed in a password. To disable this feature, enter 0.

Special character must be inside password

Select to require that special characters cannot be the first or last character.

Special characters allowed

Enter the special characters that are allowed in a password. 有关更多信息,请参阅 Password Policy .

Default characters

Click to return to the default special characters. 有关更多信息,请参阅 Password Policy .

Total minimum password length

Enter the minimum number of characters allowed in a password. To disable this feature, enter 0.

  • Password Policy
  • Configuring the Password Policy
  • Configuring the Password Policy using WebStation