WebReports Administrator is a configuration tool to configure the Reports user account in the Reports Server. The user account and password should be same in Enterprise Server and Reports Server to have proper communication between the two servers.
To transfer data from the Enterprise Server to the Reports database, the Reports user account needs to meet the following conditions:
the user account and password is the same in the Enterprise Server and the Reports Server
For more information, see Configuring Reports User Account .
the password is not expired or disabled
For more information, see Setting an Expiration Date for a User Account .
For more information, see Enabling a Disabled User Account .
the user account is associated to the Reports Administrators group
For more information, see Adding a User Account to a User Account Group .
the user account is not associated with a group with 'No Access' permission
For more information, see Editing Path Permissions of User Accounts or User Account Groups .
For more information, see Editing Command Permissions of User Account Groups .