earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Gestion des utilisateurs
Version produit : 3.2, 3.3, 2022
15/10/2020

Removing Path Permissions from User Accounts or User Account Groups

You remove a permission of an individual user account to a folder or an object when the user account no longer is to access the folder or object.

Afficher plus
action_close

​Path permissions are used to give a user account group or a user account access to the objects defined in the path. The permissions configured on a path apply to all path sub-levels unless you configure new permissions for the path sub-level.

Path permissions grant a specific set of permissions to a user account or a user account group to all the folders, sub-folders and objects contained in these folders (such as alarms, values or graphics) of a certain folder structure in the EcoStruxure Building Operations software.

The permissions defined on a path apply to all its sub-paths unless you configure new permission for a sub-path. Path permissions provided at the top level of the system are symbolized “/”. Path permissions provided to sub-levels of the system are symbolized “/[sub-level name]. Parent server is not included in the path, for instance “/Enterprise server” will only grant access to that specific server and not sub-servers.

Path Permissions Rules

A user account or a user account group can be granted the following path permissions: Read, Write, Create, Delete, Edit, Force and Command.

Pour plus d'informations, voir Path Permissions Rules .

Relative Path Permissions

Relative path permissions for a folder structure grant a specific set of permissions to a user account group or to a user account to all the folders accessible in a predefined path and its folder structure. Relative path permissions enable a user accounts group or a user account to reuse a specific path permission.

Pour plus d'informations, voir Relative Path Permissions .

To remove path permissions from a user account or user account groups
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Account management .

  4. In the account management control panel, in the Domain list box, select the domain the user account or the user account group belongs to.

  5. In the User Accounts list box or the User Account Groups list box, select the user account or the user account group, whose path permissions you want to remove.

  6. Click Software permissions .

  7. In the Permissions tab, in the Path list, select the path for which you want to remove the permissions.

  8. Click the Remove button.

  9. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Path Permissions
  • Path Permissions Rules
  • Software Permissions, User Accounts, and User Account Groups
  • Assigning Path Permissions to User Accounts or User Account Groups
  • Editing Path Permissions of User Accounts or User Account Groups