earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: WebReports
Funktionaliteter: Rapporter
Produktversion: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021-12-16

Report Manager Configuration

Before you can generate, view, and create reports in WorkStation, you need to configure certain parameters using Report Manager in WorkStation.

There are five configuration tasks:

  • Specify the URL for the WebReports Web site.

  • Specify the URL for the WebReports Web service.

  • Select the report source.

  • Verify the default report folder name.

 
action_zoom_plus_stroke Report Manager settings
Figur: Report Manager settings
Web Site URL and Web Service URL

The Web site URL specifies the WebReports Web site and includes the IP address of the Reports Server. The Web service URL points to the services that request and receive report names, and authenticate user logon information. The URLs are specified during the installation of WebReports. If you need to know what URLs to use, contact the person who installed WebReports.

After you enter the URLs and save the information, you do not need to repeat the procedure unless the location of the WebReports Web site and Web service changes at your site.

Report Source

The Report source specifies the location of the reports. You select WebReports to generate and view reports in WorkStation. The Report Pack option is not used.

Default Report Folder Name

The default Reports folder contains and organizes factory supplied reports. The folder is populated with the reports during the WebReports installation. You use the folder when you want to generate and view a factory supplied report. You also use the folder to organize custom reports.

When configuring Report Manager, keep the default setting, Reports, for the Default report folder name.

  • WebReports Overview
  • WebReports Configuration
  • Configuring Report Manager
  • Cannot Access Report Manager URL