earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: AS-P Smoke Control, Automation Server Smoke Control, Kontrola rozprzestrzeniania się dymu IP-IO, Kontrola rozprzestrzeniania się dymu MP-C, Kontrola rozprzestrzeniania się dymu MP-V
Funkcje: Smoke Control
Wersja produktu: 2022
2025-01-09

MNA-FLO-1 Enclosure

arrow1_rotationFront View arrow1_rotationInside View arrow1_rotationPhysical Dimensions arrow1_rotationMounting Dimensions

The UL 864 listed MNA-FLO-1 enclosure is a 2.75-inch deep (69.85 mm) box designed for use with VAV controllers.

Front View

The following illustration shows the front view of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Front Panel
Rysunek: MNA-FLO-1 Enclosure - Front Panel

As shown, the front view includes a product and smoke control label and an enclosure cover.

Inside View

The following illustration shows the inside view of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Inside View
Rysunek: MNA-FLO-1 Enclosure - Inside View

As shown, the inside of the enclosure includes a b3/i2865-V-S controller, an enclosure base, a damper shaft, a product label, and a mounting tab.

Physical Dimensions

The following illustration shows the physical dimensions of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Front Dimensions
Rysunek: MNA-FLO-1 Enclosure - Front Dimensions

The MNA-FLO-1 provides knockouts in the positions shown for .50 inches (12.70 mm) or .75 inches (19.05 mm) conduit connections.

Mounting Dimensions

The following illustration shows the mounting dimensions of the enclosure.

 
action_zoom_plus_stroke MNA-FLO-1 Enclosure - Mounting Dimensions
Rysunek: MNA-FLO-1 Enclosure - Mounting Dimensions
  • Smoke Control Recommended Enclosures
  • SEBOX121806 Enclosure
  • SEBOX161608 Enclosure
  • SEBOX202010 Enclosure
  • SEBOX242408 Enclosure
  • SEBOX392410 Enclosure
  • SEBOX393210 Enclosure
  • UL 864 Smoke Control Enclosure Mounting Hardware
  • Mounting a UL 864 Smoke Control Enclosure