MNA-FLO-1 Enclosure
The UL 864 listed MNA-FLO-1 enclosure is a 2.75-inch deep (69.85 mm) box designed for use with VAV controllers.
Front View
The following illustration shows the front view of the enclosure.
action_zoom_plus_stroke
图:
MNA-FLO-1 Enclosure - Front Panel
As shown, the front view includes a product and smoke control label and an enclosure cover.
The following illustration shows the inside view of the enclosure.
action_zoom_plus_stroke
图:
MNA-FLO-1 Enclosure - Inside View
As shown, the inside of the enclosure includes a b3/i2865-V-S controller, an enclosure base, a damper shaft, a product label, and a mounting tab.
Physical Dimensions
The following illustration shows the physical dimensions of the enclosure.
action_zoom_plus_stroke
图:
MNA-FLO-1 Enclosure - Front Dimensions
The MNA-FLO-1 provides knockouts in the positions shown for .50 inches (12.70 mm) or .75 inches (19.05 mm) conduit connections.
Mounting Dimensions
The following illustration shows the mounting dimensions of the enclosure.
action_zoom_plus_stroke
图:
MNA-FLO-1 Enclosure - Mounting Dimensions
Smoke Control Recommended Enclosures
SEBOX121806 Enclosure
SEBOX161608 Enclosure
SEBOX202010 Enclosure
SEBOX242408 Enclosure
SEBOX392410 Enclosure
SEBOX393210 Enclosure
UL 864 Smoke Control Enclosure Mounting Hardware
Mounting a UL 864 Smoke Control Enclosure