earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Функции: Сигналы тревоги, Базовые функции
Версия продукта: 2024, 7.0
03.12.2024

Alarm View and Event View Standard Filter and Layout

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users of the the EcoStruxure BMS.

You can edit the layout and filter conditions of the standard layout and filter provided you have write permissions on the pane or View from which you are making the changes. When you change the standard layout and filter from a pane or View, the changes are only applied on that specific pane or View and for all users who view that pane or View. Other Views in the system are not affected. You can revert your layout changes.

Standard filters in Alarm Views and Event Views support relative paths for the Source property. You can reuse the Alarm View or Event View and have the Source path of the alarms or events dynamically change depending on where you paste, import, move or duplicate the Alarm View or Event View. For example, in a relative path: '../../*' where '../' represents a folder or other container object and '*' represents anything below the folder or container object.

  • Alarms Pane and Alarm View Customization
  • Events Pane and Event View Customization
  • Saving an Alarm View Standard Layout
  • Saving an Event View Standard Layout
  • Editing an Alarm View Standard Filter
  • Editing an Event View Standard Filter
  • Displaying Alarms Assigned to the Logged On User Account
  • Displaying Alarms Assigned to the Logged On User Account Groups
  • Resetting the Alarm View Standard Layout to Factory Default
  • Resetting the Event View Standard Layout to Factory Default
  • Alarm Filters
  • Event Filter Conditions
  • Path Permissions
  • Favorites