earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Alarms, Basic Functionality
Product version: 2.0, 2.1, 3.0, 3.1
10/23/2018

Select Conditions Dialog Box

Use the Select Conditions dialog box to sort out the alarms of interest in the Alarms pane or an Alarm View , or the events in the Events pane or an Event View .

 
action_zoom_plus_stroke Select Conditions dialog box
Figure: Select Conditions dialog box

Table: Select Conditions Dialog Box

Component

Description

 
action_zoom_plus_stroke

Add condition

Select the alarm filter conditions for the alarms you want to include.

 
action_zoom_plus_stroke

Remove condition

Remove the alarm filter conditions for the alarms you want exclude.

 
action_zoom_plus_stroke

Add row

Click to add an additional row with the same condition.

 
action_zoom_plus_stroke

Remove row

Click to remove a condition row.

 
action_zoom_plus_stroke

Clear all 

Click to clear the selected conditions.

  • Alarms Pane and Alarm View
  • Events Pane and Event View
  • Alarms Pane and Alarm View Customization
  • Events Pane and Event View Customization
  • Alarm Filters
  • Event Filter Conditions
  • Add/Remove Conditions Dialog Box
  • Alarm View and Event View Standard Filter and Layout
  • Alarm Is Not Displayed in the Alarms Pane and Alarm View
  • Event Is Not Displayed in the Events Pane and Event View