earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos AS-C, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Funcionalidad básica, Gestión de usuarios
Versión del producto: 1.9
24/05/2018

Configuring Permissions to a Path

You configure the permissions users or user groups have to a path to grant or limit permissions to that path.

Mostrar más
action_close

You can manage permissions by configuring the permissions for a given user account or user account group to a certain object in the System Tree pane or List View and below that object, for example, a folder and its contents.

You need to have the required permissions to be able to view and configure user account or user group permissions to an object.

When you configure the permissions to an object, the user account and user groups that have permissions to the object are listed. You can add user accounts or user groups that you want to grant permissions to the object.

You can manually configure the permissions a user account or user group has to an object. You can also configure the object to inherit its permissons from a path above the object in the System Tree pane or List View. When you configure an object to inherit its permissions, you get an indication in the user interface that the permissions are inherited and also the specific permission level the user account or user group has to the object. You cannot configure an object to inherit the permissions from a path above this object unless you have permissions to that path.

To configure permissions to a path
  1. Select the object in the System Tree pane or List View .

  2. On the Actions menu, click Edit permissions .

     
    action_zoom_plus_stroke
  3. Click the Add users and group s button.

     
    action_zoom_plus_stroke
  4. Select the users and groups that you want grant permissions to the object path and its sub levels.

  5. Click the Add button

     
    action_zoom_plus_stroke
  6. Click OK .

  7. Configure the permission the user or group is to have to the path.

     
    action_zoom_plus_stroke
  8. Click OK .

The user or group is granted a certain permission or denied permissions to the selected object path and its sub levels.

  • Context-Sensitive Path Permissions
  • Path Permissions
  • Edit Permissions Dialog Box
  • Users and Groups Dialog Box
  • Software Permission Rules