earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: AS-C, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Server, Project Configuration Tool
Funzionalità: Gestione dell'utente
Versione del prodotto: 1.8
14/10/2016

Path Permissions Example

A user account group has the permission Full Access to the Enterprise Server and No Access to the Servers folder on the Enterprise Server. A single user account has Full Access permissions to Automation Server 1, but No Access to Automation Servers 2 and 3. The No Access permission on the Servers folders makes it possible to give specific user accounts access to specific Automation Servers in that folder.

 
action_zoom_plus_stroke Path permissions to SmartStruxure servers on different levels in Building Operation
Figura: Path permissions to SmartStruxure servers on different levels in Building Operation

The path permission rules rely on the actual path string with the name of the SmartStruxure server or folder. If you change the name of a SmartStruxure server or folder, users that earlier had permission are denied access. For example, a user group has full access to the folder LABB. The folder is renamed to Laboratory B. The users that had access to the LABB folder do not have access to the Laboratory B folder or its subfolders.

Avviso

The local admin account is always granted access on the local SmartStruxure server. Per maggior informazioni, consulta Administration Accounts in SmartStruxure Server Local Domain .

 
action_zoom_plus_stroke If you change the name of server or folder, you also have to configure the path permission to the folder.
Figura: If you change the name of server or folder, you also have to configure the path permission to the folder.

The System folder and its subfolders, except the Domains folder, are always accessible to a user even when the path permission for the folders is set to No Access. This means that a user can always at least navigate and view the objects in the System Tree and its subfolders.

Avviso

The Domains folder is the only folder within the System folder with restricted access for users with the path permission No Access.

 
action_zoom_plus_stroke The Domains folder is the only folder of the System subfolders that can be restricted by the path permission.
Figura: The Domains folder is the only folder of the System subfolders that can be restricted by the path permission.
  • Path Permissions
  • Administration Accounts in SmartStruxure Server Local Domain