Use the Basic tab to enter meter numbers, associate the meter with an extended trend log, and to add or remove tags.
Component |
Description |
Meter Reference Number |
Type the meter reference number. |
Meter Serial Number |
Type the meter serial number. |
Meter Trend Log |
Enter the path of the extended trend log you want to associate with this meter. |
Attached tags |
Displays all tags attached to the energy object. |
Enter a new tag |
Type the text you want to be displayed in a new tag. |
|
Click to place a new tag in the Attached tags area after you have entered text in the Enter a new tag box. |
|
Click to open the Add Existing Tags dialog box. For more information, see Add Existing Tags Dialog Box . |