earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: WebReports
Funktionaliteter: Rapporter
Produktversion: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021-12-16

Meter Properties – Basic Tab

Use the ​ Basic tab to enter meter numbers, associate the meter with an extended trend log, and to add or remove tags.

 
action_zoom_plus_stroke Basic tab
Figur: Basic tab

Tabell: Basic Tab

Component

Description

Meter Reference Number  

Type the meter reference number.

Meter Serial Number

Type the meter serial number.

Meter Trend Log

Enter the path of the extended trend log you want to associate with this meter.

Attached tags

Displays all tags attached to the energy object.

Enter a new tag

Type the text you want to be displayed in a new tag.

 
action_zoom_plus_stroke

Click to place a new tag in the Attached tags area after you have entered text in the Enter a new tag box.

 
action_zoom_plus_stroke

Click to open the Add Existing Tags dialog box. Mer information finns i Add Existing Tags Dialog Box .

  • Object Properties
  • Energy Monitoring Reports
  • General Information Properties – Basic Tab
  • Energy Object Tagging
  • Attaching a New Tag to an Energy Object
  • Attaching an Existing Tag to an Energy Object