Produkty: AS-P
Funkcje: Sprzęt
Wersja produktu: 2022, 2023, 2024, 7.0
2024-04-23

AS-P Server LEDs

arrow1_rotationStatus LED arrow1_rotationRS-485 LEDs arrow1_rotationEthernet LEDs arrow1_rotationLON LEDs

There are several LEDs on the front panel of an AS-P server.

The AS-P server comes in different models. The AS-P and AS-P-S models have nine LEDs whereas the AS-P-NL and AS-P-NLS models have seven LEDs.

 
action_zoom_plus_stroke  AS-P server LEDs
Rysunek: AS-P server LEDs

Tabela: The Nine LEDs

Function

Color

RS-485 A, Tx

Yellow

RS-485 A, Rx

Green

RS-485 B, Tx

Yellow

RS-485 B, Rx

Green

Ethernet 1, Link/Act/Speed

Green/Yellow

Ethernet 2, Link/Act/Speed

Green/Yellow

LON, Tx a

Yellow

LON, Mode a

Red

Status (AS-P server)

Green/Red

  1. The AS-P server models AS-P-NL and AS-P-NLS do not have LEDs for LonWorks (LON).
Uwaga

The AS-P server Ethernet and Status indicators comprise two LEDs (green/yellow and green/red respectively) in one structure. Normally, when one LED is lit, the other is not lit and vice versa, that is, the indicator will show one color at a time.

The LEDs indicate status of the AS-P server and the ongoing communication.

Status LED

The automation server Status LED indicates the condition of the device.

Tabela: Automation Server Status LED Patterns

LED Patterns

Condition

Green, constant

Normal operation, status OK

Green, flashing (~1 Hz)

Device restarting, wait

Green, flashing (~10 Hz)

Device shutting down

Red, constant

Detected error, attention required

Red, flashing (~1 Hz)

Device operates, but a problem needs attention

Red/green, flashing (~1 Hz)

Device firmware upgrade (DFU) mode or firmware being downloaded in DFU mode

No light

No input power

RS-485 LEDs

The RS-485 (COM A and COM B) LEDs indicate the condition of the RS-485 communication.

Tabela: RS-485 LED Patterns

LED Patterns

Condition

Yellow, flashing (Tx)

Transmit data

Green, flashing (Rx)

Receive data

Ethernet LEDs

The Ethernet (1 and 2) LEDs indicate the condition of the Ethernet communication.

Tabela: Ethernet LED Patterns

LED Patterns

Condition

Green, flashing

10 Mbit communication

Yellow, flashing

100 Mbit communication

LON LEDs

The LON LEDs indicate the condition of the LonWorks RS-485 communication.

Tabela: LON LED Patterns

LED Patterns

Condition

Yellow, flashing (Tx)

LON communication RS-485

Red, short flash (Mode)

During start-up; otherwise for future use

Uwaga

The AS-P server models AS-P-NL and AS-P-NLS do not have LonWorks (LON) LEDs.

  • AS-P Servers
  • Status LEDs