Notifications are used for notifying users or user groups that a certain alarm or other event, such as a schedule or an application condition, has occurred in the system. The notification contains a prewritten message that can be displayed as a popup message, sent as an email, sent to an SNMP manager, or written to a text file.
There are two types of notifications:
Alarm triggered notifications are based on alarm filter conditions that have to be met before the notification is triggered.
Variable triggered notifications are based on a variable whose condition (true, false, or both) has to be met before the notification is triggered. You can also trigger notifications manually by using the trigger notification command.
action_zoom_plus_stroke
Figure:
A notification is triggered and sends a notification report using one or more distribution methods
When setting up the notification, you configure the message text and the conditions that trigger the notification. When configuring the notification message text, you can use substitution codes to add current system information. For more information, see Alarm Substitution Codes
If you want a schedule condition to be met before the notification is enabled, you can add a schedule to the notification. For example, you only want an email to be sent on weekends. You configure the active value to match the value of a multistate schedule when the notification is to be active. This only applies for alarm triggered notifications.
In a multi-server system, a notification object created on the Enterprise Server or on the Enterprise Central notifies on alarms triggered in the child servers. The advantage of creating the notification object on the Enterprise Server or on the Enterprise Central is that you do not need to create separate notification objects for each child server server.
You can configure the notification so that it is localized to any language for which a language pack is available on the server. The default language is US English. If you choose to localize the notification, enumerations and display names are translated with the correlating names available in the language pack.
You can configure the notification to use any of the following decimal separators:
By default, the decimal separator is '.' (period).
Alarm Substitution Codes
Alarm substitution codes represent the information you want to dynamically add to alarm messages and notifications when an alarm is triggered.
For more information, see Alarms Substitution Codes
.
Notification Distribution Methods
There are four different ways to distribute a notification to a recipient:
Client
Email
SNMP
Write to File
For more information, see Notification Distribution Methods
.
Notification Reports
You can configure notification reports to include important information on the EcoStruxure BMS. Notification reports are distributed when a notification is triggered.
For more information, see Notification Reports
.
Notification Workflow
Use the notification workflow to create a notification including a notification report template.
For more information, see Notification Report Workflow
.
Date and Time Formatting
You can customize how date and time are presented in a notification text or a notification report text.
For more information, see Date and Time Formatting
.
Text Formatting
You can customize the presentation of decimals, value types, width, and alignment in a notification text or a notification report text.
For more information, see Text Formatting
.