earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 1.8
13/10/2016

Change of State Alarm Properties – Alarm Settings Tab

Use the ​ Alarm Settings tab to change the alarm properties of a change of state alarm.

 
action_zoom_plus_stroke Alarm Settings tab
Figura: Alarm Settings tab

Tabla: Alarm Settings Tab

Property

Description

Acknowledgement type

​Select the type of acknowledgement for the alarm.

Para obtener más información, consulte Acknowledgements .

Alarm message

Type the message to display when the alarm is in Alarm state.

Para obtener más información, consulte Alarm Messages .

Reset message

​Type the message to display when the alarm is reset.

Alarm priority

Enter the priority level of the alarm.

Para obtener más información, consulte Priority .

Reset priority

​Enter the priority level of the alarm when it is reset.

Para obtener más información, consulte Priority .

Category

​Enter the category that the alarm belongs to.

Para obtener más información, consulte Categories .

Cause note group

​Enter the cause note group that is used by the alarm.

Para obtener más información, consulte Cause Notes .

Action note group

​Enter the action note group that is used by the alarm.

Para obtener más información, consulte Action Notes .

Checklist

​Enter the checklist that belongs to the alarm.

Para obtener más información, consulte Checklists .

Checklist required

Select to require that a checklist is filled in before acknowledging an alarm.

Prefix for alarm source name

Type a prefix that is added to the beginning of the source name property of an alarm record.

Disable alarm

Select to disable the alarm, for example, before deployment.

Para obtener más información, consulte Habilitar y deshabilitar alarmas .

Auto hide

Select to automatically hide the alarm in the Alarms pane or Alarm View.

Para obtener más información, consulte Ocultar y mostrar alarmas .

Disable state-change logging

Select to prevent an alarm state change from creating an event.

Para obtener más información, consulte Alarm State-Change Logging .

F lashing alert

Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered.

Audible alert

Select to make the alert audible when the alarm is triggered.

 
action_zoom_plus_stroke
(Action Requirements)

Edit

Click to open the property pane where you edit the selected user action. Para obtener más información, consulte User Action Properties .

 
action_zoom_plus_stroke
(Attachments)

Add

Click to open the Create Object: Attachment wizard, where you add an attachment. Para obtener más información, consulte Create Object Wizard – Naming the Object Page .

 
action_zoom_plus_stroke
(Attachments)

Edit

Click to open the property pane where you configure the attachment. Para obtener más información, consulte Attachment Properties .

 
action_zoom_plus_stroke
(Attachments)

Remove

Click to remove an attachment that is connected to the alarm.

  • Change of State Alarms
  • Change of State Alarm Properties – Basic Tab
  • References Tab
  • Acknowledgements
  • Alarm Messages
  • Priorities
  • Categories
  • Cause Notes
  • Action Notes
  • Checklists
  • Habilitar y deshabilitar alarmas
  • Ocultar y mostrar alarmas
  • Alarm State-Change Logging
  • User Action Properties
  • Create Object Wizard – Naming the Object Page
  • Attachment Properties
  • Alarm Substitution Codes