Use the Alarm Settings tab to change the alarm properties of a matching text string alarm.
Property |
Description |
Acknowledgement type |
Select the type of acknowledgement for the alarm. Pour plus d'informations, voir Acknowledgements . |
Alarm message |
Type the message to display when the alarm is in Alarm state. Pour plus d'informations, voir Alarm Messages . |
Reset message |
Type the message to display when the alarm is reset. |
Alarm priority |
Enter the priority level of the alarm. Pour plus d'informations, voir Alarm Priority . |
Reset priority |
Enter the priority level of the alarm when it is reset. Pour plus d'informations, voir Alarm Priority . |
Category |
Enter the category the alarm belongs to. Pour plus d'informations, voir Alarm Categories . |
Category 2 |
Enter the second category the alarm belongs to. Pour plus d'informations, voir Alarm Categories . |
Cause note group |
Enter the cause note group used by the alarm. Pour plus d'informations, voir Cause Notes . |
Action note group |
Enter the action note group used by the alarm. Pour plus d'informations, voir Action Notes . |
Checklist |
Enter the checklist that belongs to the alarm. Pour plus d'informations, voir Checklists . |
Checklist required |
Select to require that a checklist is filled in before acknowledging the alarm. |
Prefix for alarm source name |
Type a prefix that is added to the beginning of the source name property of an alarm record. |
Disable alarm |
Select to disable the alarm, for example, before deployment. Pour plus d'informations, voir Désactiver et activer les alarmes . |
Auto hide |
Select to automatically hide the alarm in the Alarms pane or Alarm View. Pour plus d'informations, voir Masquer et afficher les alarmes . |
Disable state-change logging |
Select to prevent an alarm state change from creating an event. Pour plus d'informations, voir Archivage de changement d'état d'alarme . |
F lashing alert |
Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered. |
Audible alert |
Select to make the alert audible when the alarm is triggerd. |
Custom audio |
Enter the path to the custom audio file you want to play when the alarm is triggered. |
![]() |
Edit Click to open the property pane where you edit the selected user action. Pour plus d'informations, voir User Action Properties . |
![]() |
Add Click to open the Create Object: Attachment wizard where you add an attachment. Pour plus d'informations, voir Create Object Wizard – Naming the Object Page . |
![]() |
Edit Click to open the property pane where you configure the attachment. Pour plus d'informations, voir Attachment Properties . |
![]() |
Remove Click to remove an attachment that is connected to the alarm. |