earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : WorkStation
Fonctionnalités : Alarmes, Fonctionnalité de base
Version produit : 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
16/11/2018

Ajuster la largeur de la colonne aux contenus

Vous ajustez la largeur de la colonne au contenu pour afficher l'intégralité, ou une partie la plus large possible, du contenu affiché dans chacune des colonnes du volet Alarmes, de la vue Alarmes, de la Vue Événement, de la Liste de journal de tendance multiple, de la vue Liste ou Rechercher.

Afficher plus
action_close

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users of the the EcoStruxure BMS.

You can edit the layout and filter conditions of the standard layout and filter provided you have write permissions on the pane or View from which you are making the changes. When you change the standard layout and filter from a pane or View, the changes are only applied on that specific pane or View and for all users who view that pane or View. Other Views in the system are not affected. You can revert your layout changes.

Standard filters in Alarm Views and Event Views support relative paths for the Source property. You can reuse the Alarm View or Event View and have the Source path of the alarms or events dynamically change depending on where you paste, import, move or duplicate the Alarm View or Event View. For example, in a relative path: '../../*' where '../' represents a folder or other container object and '*' represents anything below the folder or container object.

Pour ajuster la largeur de la colonne aux contenus
  • Dans le volet ou la Vue , effectuez un clic droit n'importe où dans le rang des en-têtes de colonnes puis cliquez sur Adapter aux contenus .

La largeur de toutes les colonnes du volet ou de la vue est ajustée afin que tout ou la majeure partie du contenu de la colonne soit affichée.

  • Alarm View and Event View Standard Filter and Layout
  • Multi Trend Log List View