earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Modalità

Modalità


Prodotti: WorkStation
Funzionalità: Allarmi, Funzionalità di base
Versione del prodotto: 1.8, 1.9
19/07/2017

Adattamento della larghezza della colonna ai contenuti

Adatta la larghezza della colonna al contenuto per vedere tutto o buona parte del contenuto visualizzato in ogni colonna.

Mostra di più
action_close

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users in the Building Operation system.

You can edit the layout and filter conditions of the standard layout and filter provided you have write permissions on the pane or View from which you are making the changes. When you change the standard layout and filter from a pane or View, the changes are only applied on that specific pane or View and for all users who view that pane or View. Other Views in the system are not affected. You can revert your layout changes.

Standard filters in Alarm Views and Event Views support relative paths for the Source property. You can reuse the Alarm View or Event View and have the Source path of the alarms or events dynamically change depending on where you paste, import, move or duplicate the Alarm View or Event View. For example, in a relative path: '../../*' where '../' represents a folder or other container object and '*' represents anything below the folder or container object.

Per adattare la larghezza della colonna ai contenuti,
  • Nel riquadro Allarmi , riquadri Eventi , Vista allarme , Visualizza evento o Lista Trend Log Multipli fai clic con il pulsante destro del mouse in un punto qualsiasi dell'intestazione della colonna, quindi fai clic su Adatta ai contenuti .

La larghezza di tutte le colonne nel riquadro o nella visualizzazione viene adattata in modo tale che tutto o buona parte del contenuto della colonna venga visualizzato.

  • Alarms Pane and Alarm View Customization
  • Events Pane and Event View Customization
  • Alarm View and Event View Standard Filter and Layout
  • Multi Trend Log List View