earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1
2/19/2021

Notification Reports

You can configure notification reports to include important information on the EcoStruxure BMS. Notification reports are distributed when a notification is triggered.

 
action_zoom_plus_stroke Notification report
Figure: Notification report

The notification report content is configured in a notification report template that can be used and reused in notifications.

You define the contents of the notification report by configuring the following information:

  • Text adapted for the notification report

  • Events

  • Properties

  • Trend log records

  • Search results

  • Watch View properties

The notification report template text can consist of any printable characters, blank spaces, line feeds, and substitution codes.

The maximum number of trend and event records is 5000.

You configure data type groups for the events, properties, search results, trend logs, and Watch View properties you want to include in the notification report template. The data type group names become substitution codes that you can add to the notification report template. A data type group can be, for example, a list of trend log values or properties.

You can use Quick filter to find a specific substitution code in a list of available substitution codes.

An auto-complete feature helps you complete the name of a substitution code when you start typing. You can add a substitution code to the notification report template text by dragging it from the list of substitution codes.

By default, when a notification report is triggered it attempts to retrieve all the values and log data for up to 5 seconds. The timeout property is configurable.

Absolute Path or Relative Path to the Objects Connected to the Trend Log or Property

You can configure events, properties, search, trend logs, or Watch Views to point to a specific object (absolute path) or to be relative to an object (relative path).

When used in an alarm triggered notification, a relative path is relevant only when there are several identical structures of objects, for example, folders representing room or a devices. The contents of the report depend on which alarm in the structure that triggered the notification.

When used in a variable triggered notification, you can configure the path the notification report is generated relative to.

Important:

If you have more than one Relative Trend Log or Relative Properties data type group in the same notification report, you can only have one relative reference point for them all.

Example:

A notification report template including a trend log with a relative path to an alarm is used, 'Room 1'. There are two more folders in the system with content identical to the contents of the 'Room 1' folder. When an alarm is triggered in 'Room 3', the trend log data related to the triggered alarm in 'Room 3' is presented in the notification report.

Important:
  • If you use an absolute path for the property, you can move or rename the property without any data loss when the notification report is generated.

  • If you use a relative path for the property and move or rename the property, you will lose data when the report is generated.

 
action_zoom_plus_stroke Notification report with a relative path to the objects connected to the trend log or property
Figure: Notification report with a relative path to the objects connected to the trend log or property

Events Substitution Codes

Events substitution codes represent the information you want to display when a notification report is triggered. The information is dynamically filled in from the events that are included in the notification report.

For more information, see Events Substitution Codes .

Properties and Watch Substitution Codes

Properties and watch view properties substitution codes represent the information you want to display when a notification report is triggered. The information is dynamically filled in from the properties or watch view properties data that are included in the notification report.

For more information, see Properties and Watch View Properties Substitution Codes .

Trend Logs Substitution Codes

Events substitution codes represent the information you want to display when a notification report is triggered. The information is dynamically filled in from the events that are included in the notification report.

For more information, see Trend Log Records Substitution Codes .

Date and Time Formatting

You can customize how date and time are presented in a notification text or a notification report text.

For more information, see Date and Time Formatting  .

Text Formatting

You can customize the presentation of decimals, value types, width, and alignment in a notification text or a notification report text.

For more information, see Text Formatting .

Notification Report Example 1

In the example EcoStruxure BMS, we have created Building A and Building B with a number of identical rooms. Building A has three rooms: Room 1, Room 2, and Room 3. Building B has three rooms: Room 1, Room 2, and Room 3. Each room has a value and a trend log that logs the room temperature. Each room also has a value and a trend log that logs the CO 2 percentage in the air. The values are connected to alarms.

For more information, see Notification Report Example 1 .

Notification Report Example 2

In the example EcoStruxure BMS, we have created Building A and Building B with a number of identical rooms. We have also created a folder for the repeption area in Building A. In the Reception folder, we have created an analog value and a trend log that logs the temperature in the reception area. The value is connected to an alarm. A notification report that contains the log data is to be displayed in a web browser when a user manually triggers the notification.

For more information, see Notification Report Example 2 .

  • Notifications
  • Creating a Notification Report Template
  • Configuring a Notification Report Template
  • Notification Report Template View
  • Notification Report Template Properties - Basic Tab
  • Create Report Data Wizard - Configure Events Page
  • Create Report Data Wizard - Configure Properties Page
  • Create Report Data Wizard - Configure Relative Properties Page
  • Create Report Data Wizard - Configure Relative Trend Log Page
  • Create Report Data Wizard – Configure Search Page
  • Create Report Data Wizard - Configure Trend Log Page
  • Create Report Data Wizard – Configure Watch Page
  • Schedules Overview
  • Alarm Substitution Codes
  • Events Substitution Codes
  • Properties and Watch View Properties Substitution Codes
  • Trend Log Records Substitution Codes
  • Date and Time Formatting 
  • Text Formatting
  • Notification Report Example 1
  • Notification Report Example 2
  • Manually Triggering a Notification