The License Information in the Control Panel gives you an overview of the licenses in your EcoStruxure BMS.
License Information is found in the Control Panel for every EcoStruxure BMS server but the information is slightly different for every server.
Enterprise Central displays all licenses for Enterprise Central. The License Information in Enterprise Central also displays information regarding all Enterprise Servers attached to the Enterprise Central and for all field servers attached to the Enterprise Servers.
In the License Information in Enterprise Central, you can select a specific Enterprise Server and check the licenses for that server.
For more information, see EcoStruxure Building Operation Software Licensing Overview .
Enterprise Server displays all licenses for the Enterprise Server and the attached field servers.
For more information, see EcoStruxure Building Operation Software Licensing Overview .
Field server displays all licenses for products in used in the field server.
For more information, see Field Server Licensing Overview .
Licenses can have the following status:
Required : Displays the number of licenses that are required for your EcoStruxure BMS.
Used : Displays the number of licenses that are currently in use for your EcoStruxure BMS. If this number is lower than the number in Required, a license violation is displayed in the License Information. A License Violation bar is also displayed in WorkStation. For more information, see License Violation Bar .
Available : Displays the number of available licenses that are activated on the License Server but not in use in your EcoStruxure BMS.
Activated : Displays the total number of licenses that are activated on the License server, used and unused.