The License Information in the Control Panel gives you an overview of the licenses in your EcoStruxure BMS.
It is recommended that you use one separate License server for every Enterprise Central and Enterprise Server. It is easier to get an overview of your licenses if you use a dedicated server for every Enterprise Central and Enterprise Server.
If two or more Enterprise Servers gets their licenses from the same license server, you cannot identify which Enterprise Server got the license.
Using a License Administrator on the same computer as the Enterprise Server or Enterprise Central makes your system less vulnerable to network failure.
If you do not use the recommended setup you get the system alarm "Invalid license server configuration".
The License Information is found in the Control Panel for every EcoStruxure BMS server but the information is slightly different for every server.
The Enterprise Central displays all licenses for the Enterprise Central. The License Information in Enterprise Central also displays information regarding all Enterprise Servers attached to the Enterprise Server and for all SmartX servers attached to the Enterprise Servers.
In the License Information in Enterprise Central you can select a specific Enterprise server and check the licenses for that server.
Enterprise server displays all licenses for the Enterprise Server and the attached SmartX servers.
SmartX server displays all licenses for products in used in the SmartX server.
Pour plus d'informations, voir Device Administrator Licenses .
Licenses can have the following status:
Required : Displays the number of licenses that are required for your EcoStruxure BMS.
Used : Displays the number of licenses that are currently in use for your EcoStruxure BMS. If this number is lower than the number in Required, a license violation is displayed in the License Information. You also get a license violation bar in WorkStation. Pour plus d'informations, voir License Violation Bar .
Available : Displays the number of available licenses that are activated on the License Server but not in use in your EcoStruxure BMS.
Activated : Displays the total number of licenses that are activated on the License server, used and unused.