earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-P Smoke Control, Automation Server Smoke Control
功能: 烟气控制
产品版本: 2024
2025/1/9

Electronics Module Installation

To ensure that the correct electronics module is used with the correct terminal base, you must always check that the warning label on the terminal base backplane indicates which module type should be connected. Write the intended module type, if it is not already printed, on the label.

 
action_zoom_plus_stroke Terminal Base Label (Module Type)
图: Terminal Base Label (Module Type)
警告 警告

意外设备操作

Install only the module type that is indicated on the label of the terminal base. If the label does not indicate the intended module type, consult the control panel documentation to determine the intended module type. A mismatch can cause electric shock and damage the electronics module.

不遵守这些说明将导致死亡、严重伤害或设备损坏。

Install an electronics module on a terminal base as follows:

1. Pull out the two handles on the left and right sides of the module

2. Plug the module into the terminal base, ensuring that the PCB header pins align correctly with the backplane socket, and press firmly

3. Push the handles in firmly to lock the module in place

4. Open the clear plastic label carriers

5. Write and insert the labels

6. Close the label carriers

If the PS-24V module is inserted with 24 VAC power applied, the Smoke Control, or Central IO module you are installing powers up when plugged in. You should see the status LED activate. 有关更多信息,请参阅 PS-24V Power Supply Module .

  • EcoStruxure BMS Module Installation
  • Terminal Base Installation
  • Power Rating
  • Terminal Base Wiring
  • PS-24V Power Supply Module
  • Automation Server Installation
  • AS-P and AS-P-NLS Installation
  • RS-485 Field Bus Cable Routing
  • Module and MP Controller Status LEDs
  • Central IO Module Installation