In WorkStation you can customize your workspace to some extent. You can, for example, decide where workspace components, such as, Alarms are displayed.
You can configure the workspace layout, for example, to display different workspace items on different monitors or to change the size of a pane to improve readability. When you save the modified workspace layout, it is saved on the local computer. If you log on to WorkStation on another computer you cannot access the customized layout. The modified workspace layout is displayed the next time you log on to WorkStation.
You can switch the following bars on or off:
Address bar
Menu bar
Toolbar
Status bar
Search bar
History bar
For each window, pane, or work area in the workspace the user can modify the following:
Auto hide on/off
Closed on/off
Floating on/off
Position
You can reset a modified workspace layout on the local computer. In this case, you return to the default workspace layout that applies for your user account.