earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WorkStation
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Showing a Hidden Main Menu

You show a hidden main menu when you want it to be visible.

Pokaż więcej
action_close

In WorkStation you can customize your workspace to some extent. You can, for example, decide where workspace components, such as, Alarms are displayed.

You can configure the workspace layout, for example, to display different workspace items on different monitors or to change the size of a pane to improve readability. When you save the modified workspace layout, it is saved on the local computer. If you log on to WorkStation on another computer you cannot access the customized layout. The modified workspace layout is displayed the next time you log on to WorkStation.

You can switch the following bars on or off:

  • Address bar

  • Menu bar

  • Toolbar

  • Status bar

  • Search bar

  • History bar

For each window, pane, or work area in the workspace the user can modify the following:

  • Auto hide on/off

  • Closed on/off

  • Floating on/off

  • Position

You can reset a modified workspace layout on the local computer. In this case, you return to the default workspace layout that applies for your user account.

To show a hidden Main menu
  • In WorkStation, right-click the toolbar and then select Main menu .

  • Customization
  • WorkStation Overview
  • Hiding Menus and Toolbars