earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2.0, 2.1, 3.0, 3.1
16/01/2019

Saving an Event View Standard Layout

You save a standard layout to make a change to the Events pane or an Event View layout available to all users.

Afficher plus
action_close

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users of the the EcoStruxure BMS.

You can edit the layout and filter conditions of the standard layout and filter provided you have write permissions on the pane or View from which you are making the changes. When you change the standard layout and filter from a pane or View, the changes are only applied on that specific pane or View and for all users who view that pane or View. Other Views in the system are not affected. You can revert your layout changes.

Standard filters in Alarm Views and Event Views support relative paths for the Source property. You can reuse the Alarm View or Event View and have the Source path of the alarms or events dynamically change depending on where you paste, import, move or duplicate the Alarm View or Event View. For example, in a relative path: '../../*' where '../' represents a folder or other container object and '*' represents anything below the folder or container object.

To save an Event View standard layout
  1. In WorkStaton, in the Events pane or an Event View, right-click anywhere in the column header row and then click Add/Remove columns .

  2. Select the columns that you want to add or clear columns that you want to remove from the Alarm View standard layout.

  3. Click OK .

  4. Move the Events pane or Event View columns to the position where you want them by dragging the column heading.

  5. Click the arrow that appears next to a column heading to choose ascending or descending alphanumeric sort order for the content of that column.

  6. Right-click the column heading row and select Group box

     
    action_zoom_plus_stroke
    .

  7. Drag a column heading to the group box to group the events by that category.

     
    action_zoom_plus_stroke
  8. Right-click anywhere in the Events pane or Event View, point to Event View settings and then click Save as standard layout .

The standard layout is applied on the Events pane or the Event View from which you made the changes and is applied when a user opens the Events pane or Event View.

  • Alarm View and Event View Standard Filter and Layout
  • Events Pane and Event View Customization
  • Regrouper et trier des objets
  • Add/Remove Columns Dialog Box (Events)
  • Menu contextuel du volet Événements - Sous-menu Paramètres de vue Événements
  • Resetting the Event View Standard Layout to Factory Default