earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2023
17/12/2022

Editing an Event View Standard Filter

You edit a standard filter to narrow what is displayed in the Events pane or an Event View for all users in the EcoStruxure Building Operation software.

Afficher plus
action_close

A standard layout defines the columns that are included in the Alarms pane, Events pane, Alarm View, or Event View, the order in which they are displayed, whether or not the alarms or events are grouped in any way and whether they are displayed in an ascending or descending order. A standard filter defines the conditions that have to be met before the alarms or events are displayed in the pane or a View. The standard layout and filter is saved for the pane or View to which you made the changes. The standard layout and filter is displayed for all users of the the EcoStruxure BMS.

You can edit the layout and filter conditions of the standard layout and filter provided you have write permissions on the pane or View from which you are making the changes. When you change the standard layout and filter from a pane or View, the changes are only applied on that specific pane or View and for all users who view that pane or View. Other Views in the system are not affected. You can revert your layout changes.

Standard filters in Alarm Views and Event Views support relative paths for the Source property. You can reuse the Alarm View or Event View and have the Source path of the alarms or events dynamically change depending on where you paste, import, move or duplicate the Alarm View or Event View. For example, in a relative path: '../../*' where '../' represents a folder or other container object and '*' represents anything below the folder or container object.

To edit an Event View standard filter
  1. In WorkStation, right-click anywhere in the Events pane or Event View, point to Event View settings, and then click Edit standard filter .

  2. In the Add/Remove Conditions dialog box, click the Add condition button

     
    action_zoom_plus_stroke
    .

  3. In the Select Conditions dialog box, select the conditions you want to add to the Events pane or Event View standard filter.

  4. Click OK .

  5. Click the Add row button

     
    action_zoom_plus_stroke
    to add another row for the same condition.

  6. Enter the sub condition that has to be met before the event is displayed in the Events pane or Event View.

  7. Click OK .

The standard filter is applied for all users who open the changed Events pane or Event View.

  • Alarm View and Event View Standard Filter and Layout
  • Events Pane and Event View Customization
  • Event Filter Conditions
  • Sélectionner la boîte de dialogue Conditions
  • Saving an Event View Standard Layout
  • Menu contextuel du volet Événements - Sous-menu Paramètres de vue Événements
  • Resetting the Event View Standard Layout to Factory Default