earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos AD v2, AD v1
Funcionalidades: Hardware
Versión del producto: 3.3, 2022, 2023, 2024
23/07/2021

Connecting an Advanced Display to an AS-P server or AS-B server

You connect an Advanced Display to a AS-P server or AS-B server in order to communicate with EcoStruxure BMS servers over a USB connection, to supply the Advanced Display with power, and to ensure that its battery is charged.

Mostrar más
action_close

AD v2 uses a wired (USB) connection to communicate with EcoStruxure BMS servers. During installation and commissioning, you can use a wireless access point to establish communication between AD v2 and EcoStruxure BMS servers. AD v2 can be powered either by a AS-P server, AS-B server, or USB power adapter.

Communication over a USB Connection

The preinstalled AD-Link application enables AD v2 to communicate with EcoStruxure BMS servers over a USB connection.

When AD v2 is connected to a AS-P server or AS-B server, AD v2 can be powered by the automation server through the USB cable. The screen must not be turned on constantly because this may drain the battery.

Aviso

LOSS OF DATA OR POWER

  • Use only USB cables ordered from Schneider Electric.

  • Use only USB cables that are designed for AD.

  • Do not use USB cables that exceed 3 m (10 ft).

Failure to follow these instructions can result in loss of data or power.

 
action_zoom_plus_stroke USB connection to a AS-P server or AS-B server
Figura: USB connection to a AS-P server or AS-B server

To connect an Advanced Display to an AS-P server or AS-B server
  1. Insert the USB cable from the Advanced Display into the USB host port on the AS-P server or AS-B server.

    Aviso

    Connect only one Advanced Display to an AS-P server or AS-B server. The USB host port can supply only one Advanced Display with power. Connecting several Advanced Displays to an AS-P server or AS-B server can cause the Advanced Displays to lose performance, shut down, or discharge their batteries.

  2. If an Attention message “Unable to find software on your computer that can recognize your device...” appears on the Advanced Display, ignore the message and tap OK .

  3. Ensure that the screen timeout is configured to automatically turn off the screen when you are not using the device, because the sleep mode is used to fully charge the battery.

  • AD v2 Communication and Power
  • AD v1 Communication and Power
  • Installing the AD v2 Tablet and Frame
  • Installing the AD v1 Tablet and Frame
  • AD v1 or AD v2 Does Not Turn On or Battery Does Not Charge
  • AD v1 or AD v2 Battery Does Not Fully Charge
  • USB Data Communication is Lagging or Data is Lost