earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

System Alarm Handling

System alarms are usually handled similarly to other alarms. After acknowledging a system alarm, the cause of the alarm must be corrected before the alarm state changes to reset and then returns to normal state.

 
action_zoom_plus_stroke System alarm acknowledgement loop where the alarm is acknowledged in alarm state
图: System alarm acknowledgement loop where the alarm is acknowledged in alarm state
 
action_zoom_plus_stroke System alarm acknowledgement loop where the alarm is acknowledged in reset state
图: System alarm acknowledgement loop where the alarm is acknowledged in reset state

Simple system alarms are system alarms with a simplified state handling. When you acknowledge a simple system alarm, it disappears from the Alarms pane, regardless of the current alarm state. For example, a simple system alarm notifies the user when a EcoStruxure BMS server or field device performs a warm start.

 
action_zoom_plus_stroke Simple system alarm acknowledgement loop where the alarm is acknowledged in alarm state
图: Simple system alarm acknowledgement loop where the alarm is acknowledged in alarm state
  • System Alarms
  • Alarm States
  • Acknowledgements
  • Notifications
  • System Alarm ID List