Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base, Sécurité
Version produit : 2024, 7.0
03/12/2024

Adding a File Extension to the Permitted File Extensions List

You add a file extension to the Permitted File Extensions list so that EcoStruxure Building Operation users can open, save, and import files with that file extension.

Afficher plus
action_close

You can increase the security in your system by configuring the document policy. The document policy controls which file types a user can open, save, and import.

You configure the document policy by determining the permitted file extensions for the EcoStruxure BMS. A user cannot open, save, or import files with file extensions that are not on the list. A user can save a file without any file extension.

A user who browses the system to create or edit a document object can only see files with permitted file extensions and files without any file extension.

By default, the list of permitted file extensions contains the following file extensions:

  • avi

  • dfx

  • doc

  • docx

  • dwg

  • gif

  • htm

  • html

  • jpg

  • mp4

  • mpg

  • odt

  • pdf

  • png

  • rtf

  • txt

  • vsd

  • xls

  • xlsx

The permitted file extensions list configuration on an Enterprise Server is distributed to all field servers in the EcoStruxure BMS.

You can add file extensions to, and delete file extensions from, the permitted file extensions list. If you have configured the list, it is preserved when you upgrade the EcoStruxure BMS.

If a file extension is not on the permitted file extensions list and a user performs a restore operation, the operation succeeds and the document object is restored, but it is no longer possible to open the document file. If the document file extension is added to the permitted file extensions list, it is possible to open and save the restored document file.

If you upgrade an older EcoStruxure BMS without a document policy, the upgraded system gets the default document policy.

To add a file extension to the Permitted File Extensions list
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Under Security and communication , click Document Policy .

  4. In the Document Policy view, click the Add file extension button

     
    action_zoom_plus_stroke
    .

  5. In the Add File Extension dialog box, in the File extension box, type the file extension you want to add to the list and then click OK .

    Déclaration

    Do not use a period '.' in the file extension. For example, type 'pdf' rather than '.pdf'.

  6. Click the Save button

     
    action_zoom_plus_stroke
    .

An EcoStruxure Building Operation user can open, save, or import files with the added file extension.

  • Document Policy
  • Document Policy View
  • Add File Extension Dialog Box
  • Editing a File Extension on the Permitted File Extensions List 
  • Removing a File Extension from the Permitted File Extensions List