earth_america
user_standard Anmelden
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Ratgeber

Ratgeber


Produkte: AS-C, AS-B, Enterprise Server, AS-P, Projekt Configuration Server, Project Configuration Tool
Funktionen: Basisfunktionalität, Sicherheit
Produktversion: 1.8
13.10.2016

Removing a File Extension from the Permitted File Extensions List

You remove a file extension from the Permitted File Extensions list to increase the security of your Building Operation system by preventing users from opening, saving, and importing files with a certain file extension.

Mehr zeigen
action_close

You can increase the security in your system by configuring the document policy. The document policy controls which file types a user can open, save, and import.

You configure the document policy by determining the permitted file extensions for the Building Operation system. A user cannot open, save, or import files with file extensions that are not on the list. A user can save a file without any file extension.

A user who browses the system to create or edit a document object can only see files with permitted file extensions and files without any file extension.

By default, the list of permitted file extensions contains the following file extensions:

  • avi

  • dfx

  • doc

  • docx

  • dwg

  • gif

  • htm

  • html

  • jpg

  • mp4

  • mpg

  • odt

  • pdf

  • png

  • rtf

  • txt

  • xls

  • xlsx

The permitted file extensions list configuration on an Enterprise Server is distributed to all SmartStruxure Server devices in the Building Operation system.

You can add file extensions to, and delete file extensions from, the permitted file extensions list. If you have configured the list, it is preserved when you upgrade the Building Operation system.

If a file extension is not on the permitted file extensions list and a user performs a restore operation, the operation succeeds and the document object is restored, but it is no longer possible to open the document file. If the document file extension is added to the permitted file extensions list, it is possible to open and save the restored document file.

If you upgrade an older Building Operation system without a document policy, the upgraded system gets the default document policy.

In Project Configuration Server, if you have not added a SmartStruxure server to your project, the default permitted file extensions list is applied. When you have added a SmartStruxure server to your project and edited the permitted file extensions list for that server, the changes are applied on Project Configuration Server as well.

To remove a file extension from the Permitted File Extensions list
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. Under Security and communication , click Document Policy .

  3. On the Permitted File Extensions list, select the file extension you want to remove.

  4. Click the Remove file extension button

     
    action_zoom_plus_stroke
    .

     
    action_zoom_plus_stroke
  5. Click the Save button

     
    action_zoom_plus_stroke
    .

A user in the Building Operation system can no longer open, save, or import a file with extension that you deleted from the Permitted File Extensions list.

  • Document Policy
  • Document Policy View
  • Document Policy Toolbar
  • Adding a File Extension to the Permitted File Extensions List
  • Editing a File Extension on the Permitted File Extensions List