earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-P-3, AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Trends
Product version: 7.0, 7.1
10/30/2025

Multi Trend Log Settings Dialog Box – General Tab

Use the General tab to edit the properties that control how all the trend log series are presented in a multi trend log list.

Important:

Changes made on the General tab override settings made on individual series on the Series tab.

 
action_zoom_plus_stroke General tab
Figure: General tab

Table: Multi Trend Log Settings – General Tab

Property

Description

Log space (records)

​Select the maximum number of records to display in the list.

Time zone

Select the time zone in which the log records are presented.

Calculation method

Select a calculation method.

For more information, see Calculation Methods .

Delta over period

Select True to apply a period to the delta calculation method.

For more information, see Calculation Methods .

Period  

Select the time span for which the calculation method is to be executed.

Custom period

Enter a custom time span for which the calculation method is to be executed.

Custom period alignment

Enter the time when you want the custom period to start.

  • Multi Trend Log Lists
  • Multi Trend Log List View
  • Time Zone Modes in a Trend Log List
  • Calculation Methods
  • Multi Trend Log Settings Dialog Box – Series Tab
  • Multi Trend Log List Properties - Basic Tab