earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-P-3, AS-B, Edge Server, Enterprise Central, Enterprise Server, ​License Administrator, ​License Server, AS-P, WorkStation, WebStation
Functionalities: Basic Functionality, Engineering, License Management
Product version: 7.0, 7.1
10/30/2025

License Enforcement and Information

arrow1_rotationLicense Violation arrow1_rotationLicense Expiration arrow1_rotationLicense Information

License enforcement is the process of checking whether a software application has a valid license available to it at runtime. If you do not have enough licenses, a license violation is displayed in the License Information bar in WorkStation and WebStation.

For more information, see Software and Features that Require Licenses .

License Violation

The first time you add an additional device to the Enterprise Server, other than a field server, in excess of the number of licenses purchased, a license violation is displayed in the License Information bar.

The system information alarm, License Violation, is triggered at the same time as the license violation is displayed.

To get more specific information regarding the licenses, click on Licensing Information.

 
action_zoom_plus_stroke License Information bar in WorkStation when a violation has occurred.
Figure: License Information bar in WorkStation when a violation has occurred.

For more information, see License Information Bar .

License Expiration

If a license has expired or is set to expire within 30 days, a license expiration or a license renewal reminder with information on the expiration date is displayed in the Licenses Information bar. To see specific information about your licenses, click Licensing Information.

License Information

When you use Demo licenses or Engineering licenses you are notified in the License Information and Enforcement bar.

For more information, see Demo Licenses and Engineering Licenses .

  • Licenses Administrated by License Administrator Overview
  • Demo Licenses and Engineering Licenses
  • License Information Bar