earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, License Administrator, License Server, AS-P, WorkStation, WebStation
Fonctionnalités : Fonctionnalité de base, Ingénierie, Gestion des licences
Version produit : 2024
02/12/2024

License Enforcement

arrow1_rotationLicense Violation

License enforcement is the process of checking whether a software application has a valid license available to it at runtime. If you do not have enough licenses, a license violation occurs. This is accomplished by a license violation bar in WorkStation and WebStation.

If a client, such as WorkStation or one of the editors, attempts to start and cannot locate an available license, the client does not start.

Pour plus d'informations, voir Software and Features that Require Licenses .

License Violation

The first time you add an additional device to the Enterprise Server, other than a field server, in excess of the amount of licenses purchased, a license violation bar is displayed. The license violation bar states that you have exceeded the amount of licenses available, and urges you to purchase the additional licenses required. The license violation bar displays every time you log on to the system, and is displayed on all WorkStations and WebStations that are logged into the system.

The system information alarm, License Violation, is triggered at the same time as the License Violation bar is displayed.

To get more specific information regarding the licenses, you can click on Licensing Information. Pour plus d'informations, voir License Information Enterprise Server .

 
action_zoom_plus_stroke License violation bar in WorkStation
Figure : License violation bar in WorkStation

Pour plus d'informations, voir License Violation Bar .

  • EcoStruxure Building Operation Software Licensing Overview
  • License Information Enterprise Server
  • License Violation Bar