earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 3.2, 3.3, 2022
10/15/2020

Variable Triggered Notification Properties - Basic Tab

Use the Basic tab to view or edit the properties of the variable triggered notification.

 
action_zoom_plus_stroke Variable triggered notification properties
Figure: Variable triggered notification properties

Table: Variable Triggered Notification

Property

Description

Trigger variable

Enter the variable that triggers the notification.

Trigger condition

Select when you want the notification to be triggered: when the trigger variable changes to true, changes to false, or all changes.

Report template

Enter the path to the report template.

For more information, see Notification Reports .

Generate report relative to

Enter the path to the object that is relative to the generated notification report.

Decimal symbol

Select the decimal symbol to be used in the notification and the notification report template.

Localization

Select a language among the language packs installed on the EcoStruxure BMS server.

System of measurement

Select the system of measurements to be used in the notification report.

Report format

Select the format of the notification report.

XLSX template

Enter the path to the XSLX notification report template.

Notification text

Edit the notification text.

 
action_zoom_plus_stroke

Add

Click to add a distribution method to the notification.

For more information, see Notification Distribution Methods .

 
action_zoom_plus_stroke

Edit

Click to configure the selected distribution method in the notification.

For more information, see Notification Distribution Methods .

 
action_zoom_plus_stroke

Remove

Click to remove the selected distribution method from the notification.

For more information, see Notification Distribution Methods .

  • Notifications
  • Notification Reports
  • Notification Distribution Methods
  • References Tab
  • General Information Properties – Basic Tab