earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 2.0, 2.1, 3.0, 3.1
05/01/2019

Variable Triggered Notification Properties - Basic Tab

Use the Basic tab to view or edit the properties of the variable triggered notification.

 
action_zoom_plus_stroke Variable triggered notification properties
Figura: Variable triggered notification properties

Tabla: Variable Triggered Notification Properties

Property

Description

Trigger variable

Enter the variable that triggers the notification.

Trigger condition

Select when you want the notification to be triggered: when the trigger variable changes to true, changes to false, or all changes.

Report template

Enter the path to the report template.

Para obtener más información, consulte Notification Reports .

Generate report relative to

Enter the path to the object that is relative to the generated notification report.

Decimal symbol

Select the decimal symbol to be used in the notification and the notification report template.

Localization

Select a language among the language packs installed on the EcoStruxure BMS server.

Notification text

Edit the notification text.

 
action_zoom_plus_stroke

Add

Click to add a distribution method to the notification.

Para obtener más información, consulte Notification Distribution Methods .

 
action_zoom_plus_stroke

Edit

Click to configure the selected distribution method in the notification.

Para obtener más información, consulte Notification Distribution Methods .

 
action_zoom_plus_stroke

Remove

Click to remove the selected distribution method from the notification.

Para obtener más información, consulte Notification Distribution Methods .

  • Notifications
  • Notification Reports
  • Notification Distribution Methods
  • References Tab
  • General Information Properties – Basic Tab