Use the Basic tab to view or edit the properties of the variable triggered notification.
Property |
Description |
Trigger variable |
Enter the variable that triggers the notification. |
Trigger condition |
Select when you want the notification to be triggered: when the trigger variable changes to true, changes to false, or all changes. |
Report template |
Enter the path to the report template. Per maggior informazioni, consulta Notification Reports . |
Generate report relative to |
Enter the path to the object that is relative to the generated notification report. |
Decimal symbol |
Select the decimal symbol to be used in the notification and the notification report template. |
Localization |
Select a language among the language packs installed on the EcoStruxure BMS server. |
System of measurement |
Select the system of measurements to be used in the notification report. |
Report format |
Select the format of the notification report. |
XLSX template |
Enter the path to the XSLX notification report template. |
Notification text |
Edit the notification text. |
|
Add Click to add a distribution method to the notification. Per maggior informazioni, consulta Notification Distribution Methods . |
|
Edit Click to configure the selected distribution method in the notification. Per maggior informazioni, consulta Notification Distribution Methods . |
|
Remove Click to remove the selected distribution method from the notification. Per maggior informazioni, consulta Notification Distribution Methods . |