earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Alarmes
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Notification Report Template Properties - Basic Tab

Use the Basic tab to view or edit the properties of the notification report template.

 
action_zoom_plus_stroke Notification Report Template properties
Imagem: Notification Report Template properties

Tabela: Notification Report Template Properties

Property

Description

Report data

Use Report data to add, edit, or remove data type groups to the notification report template.

 
action_zoom_plus_stroke

Add  

Click to add a report data type to the notification report template.

 
action_zoom_plus_stroke

Edit  

Click to edit the properties of the selected report data type.

 
action_zoom_plus_stroke

Remove  

Click to remove the selected report data type.

Report text

Enter text to include in the notification report template.

First day of week

Select the day to be set as the first day of week.

Time zone

Select the time zone for the notification reports.

Timeout(s)

Enter the number of seconds the notification attempts to fetch values from the EcoStruxure Building Operation database before canceling.

  • Notification Reports
  • References Tab
  • General Information Properties – Basic Tab