earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, License Administrator, License Server, AS-P, WorkStation, WebStation
Funcionalidades: Funcionalidad básica, Gestión de licencias
Versión del producto: 2.0, 2.1, 3.0, 3.1
18/05/2018

Field Bus Device Licenses

All field bus devices hosted by an EcoStruxure Building Operation Enterprise Server need licenses.

The hosting allocation is performed on a per site basis, and all licenses are controlled by the Enterprise Server.

Any field bus device that is hosted by an EcoStruxure Building Operation Enterprise Server and can be configured without the use of some legacy tool requires a license to be available. The following field bus devices require a license:

  • BACnet IP devices

  • MNB 1000 devices

  • LonWorks devices

  • Modbus TCP devices

  • Licensing Model
  • Licensing Enforcement