earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, ​License Administrator, ​License Server, AS-P, WorkStation, WebStation
功能: 基本功能, 许可证管理
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Field Bus Device Licenses

All field bus devices hosted by an EcoStruxure Building Operation Enterprise Server need licenses.

The hosting allocation is performed on a per site basis, and all licenses are controlled by the Enterprise Server.

Any field bus device that is hosted by an EcoStruxure Building Operation Enterprise Server and can be configured without the use of some legacy tool requires a license to be available. The following field bus devices require a license:

  • BACnet IP devices

  • MNB 1000 devices

  • LonWorks devices

  • Modbus TCP devices

  • Licensing Model
  • Licensing Enforcement