Use the Configure Email page to configure the email properties of the notification.
Component |
Description |
Subject |
Type the subject text or the substitution code for the subject text the email notification is to have when sent. |
To users and groups |
Click the browse button to open the Users and Groups dialog box where you select the EcoStruxure Building Operation users or user groups to whom the email notification is to be sent. 有关更多信息,请参阅 Users and Groups Dialog Box . |
To email address |
Type the email address of an alternative recipient. |
Send as attachment |
Select to add send the notification as an attachment in the email. |
Attchment filename |
Type a file name for the notification attachment. |
|
Click to open the Configure dialog box where you configure a reference for a dynamic attachment file name. 有关更多信息,请参阅 Configure Dialog Box – Configuration Tab . |