earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 3.2, 3.3, 2022
10/15/2020

Alarm Triggered Notification Properties - Basic Tab

Use the Basic tab to view or edit the properties of the alarm triggered notification.

 
action_zoom_plus_stroke Alarm triggered notification properties
Figure: Alarm triggered notification properties

Table: Alarm Triggered Notification

Property

Description

Status

Select Disabled to deactivate the notification function.

Activation schedule

Enter the schedule that contains the value that activates the notification.

Schedule value when active

Enter the value, generated by the connected schedule or other multistate variable, that activates the notification.

Report template

Enter the path to the report template.

For more information, see Notification Reports .

Decimal symbol

Select the decimal symbol to be used in the notification and the notification report template.

Localization

Select a language among the language packs installed on the EcoStruxure BMS server.

System of measurment

Select the system of measurements to be used in the notification report.

Report format

Select the format of the notification report.

XLSX template

Enter the path to the XSLX notification report template.

Notification text

Edit the notification text.

Substitute missing data with

Enter the text that is displayed when a value is missing. By default, a missing value displays nothing at all.

 
action_zoom_plus_stroke

Add

Click to add a distribution method to the notification.

For more information, see Notification Distribution Methods .

 
action_zoom_plus_stroke

Edit

Click to configure the selected distribution method in the notification.

For more information, see Notification Distribution Methods .

 
action_zoom_plus_stroke

Remove

Click to remove the selected distribution method from the notification.

For more information, see Notification Distribution Methods .

Notify on transition to

Select the alarm states that trigger the notification.

 
action_zoom_plus_stroke

Click to add an alarm filter condition for the notification. For more information, see Alarm Filters .

 
action_zoom_plus_stroke

Click to remove the selected alarm filter conditions for the notification.

 
action_zoom_plus_stroke

Clear all

Click to remove all the alarm filter conditions for the notification.

  • Notifications
  • Notification Reports
  • Notification Distribution Methods
  • References Tab
  • General Information Properties – Basic Tab