earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funktionaliteter: Larm
Produktversion: 3.2, 3.3, 2022
2024-05-06

Write to File Notification Distribution Method

The write to file notification is written to a text file or to an XLSX file when the configured notification condition is met.

You can configure whether new information is appended to the existing file, overwrites the current content of the file, or if it is written to a unique file. By default, new information is appended to the existing file. If the file does not exist, a new text file is created.

You can make the file name dynamic by replacing it with a string variable whose value you control from a program.

The text file or an XLSX file, or a PDF file is saved in the EcoStruxure Building Operation database folder: '...db/notifications'. This location cannot be changed.

You access the notification file from the WorkStation 'System' folder, 'Notification files' subfolder of the EcoStruxure BMS server where the file was generated. You can open the notification file with a text editor or an XLSX file editor, or a PDF file reader installed on the computer.

You can save the notification file, from the WorkStation 'System' folder, 'Notification files' subfolder, to a different location and rename it. You can also delete the notification file.

Obs!

When you delete the notification file, it is deleted from the physical device.

  • Notification Distribution Methods
  • Create Object Wizard - Configure Write to File Page
  • Accessing a Notification Written to a File
  • Saving a Notification Written to a File
  • Deleting a Notification Written to a File
  • Email Notification Distribution Method
  • SNMP Notification Distribution Method
  • XML Notation for Substitution Codes in XLSX Report Template