功能: 警报
产品版本: 1.8
2016/10/13

SNMP Notification Distribution Method

SNMP alarms are typically used when the alarm receiver does not have access to Building Operation software or when a central unit, for example the IT department, wants to collect alarms from different sources in one place.

You can send notifications as SNMP traps from any SmartStruxure server using SNMP version 3. The SmartStruxure server can send one or many traps depending on the setting.

You configure the SNMP trap to send the notification message.

Notifications sent using SNMP trap are written to the event log.

SNMP is also used to send information regarding the status of a SmartStruxure server device. 有关更多信息,请参阅 SmartStruxure Server Devices ..

  • Notification Distribution Methods
  • Create Notification Wizard - Configure SNMP Page
  • SmartStruxure Server Devices
  • Email Notification Distribution Method
  • Write to File Notification Distribution Method